Part Number: AM4378
Other Parts Discussed in Thread: TPS65218
Hi,
Let me talk about Power consumption of AM437x and TPS65218.
Power consumption of CAP_VDD_RTC and VDDS_RTC are described in AM437x datasheet.
They are Max 2 and 5mA
but Power consumption of DCDC5/6's output current is described in TPS65218 datasheet.
It is Max 100μA
(1)In this case, I want to confirm maximum current value consumed by the RTC of AM 437x.
(2)Can AM437x accept this current worst case at battery backup of RTC?
Best Regards
Hiroyasu