Part Number: AM5716
Other Parts Discussed in Thread: TPS650250,
Hi,
Ti implements clamp circuits for the 3.3V rail to ramp down this rail simultaneous with the 1.8V rail preventing the 3.3V rail from beeing 2V higher than the 1.8V rail.
I have seen an implementation of this in the AM571x IDK EVM as well as in an AM335x/TPS650250 documentation (slvu731a). The implementation in the AM571x IDK EVM has recently been modified to address tolerance issues of the two power rails. Despite of this there is a small structural difference in the implementation (please see pictures).
R1 is directly on the 3.3V rail in one solution. In the other one this resistor is indirectly connected to the 3.3V rail with the 499Ohm resistance.
Is there any advantage of doing the circuit in one or the other way?
Thanks and best regards,
Patrick