This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Videomixer timestamping problem

Part Number: AM5728


Hi,

I am trying to overlay a buffer of PNG images in real-time to a h264 encoded video stream. I am testing with the following pipeline:

gst-launch-1.0 -v videotestsrc ! video/x-raw, width=800, height=480, framerate=30/1 ! \
ducatih264enc ! decodebin ! \
video/x-raw, format=NV12 ! vpe ! video/x-raw, format=RGB ! \
videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! \
waylandsink sync=true \
multifilesrc location="img.%04d.png" index=0 stop-index=1 loop=true caps="image/png,framerate=\(fraction\)30/1" ! pngdec ! videorate ! mix.

When waylandsink sync=true, the video stream framerate on the EVM is very low and the message appears:

There may be a timestamping problem, or this computer is too slow.

When waylandsink sync=false, the video stream framerate is still very low, but it seems to capture every frame and remove the message above, but display it with extremely high latency.

I was not able to successfully change decodebin to use ducatih264dec, not sure why. The CPU usage between the two cores is about 50/50, so I think the issue may be with timestamping. Am I missing some caps, or what can I add to resolve the timestamping issue?

Thanks,

Vishal

  • Hello,

    I would recommend you to add queue elements in the pipeline, set sync=false and set caps filters with height, width,  etc.

    Vishal said:
    I was not able to successfully change decodebin to use ducatih264dec, not sure why.

    Did you add parser element between dec and enc?

    BR
    Margarita

  • Hi Margarita,

    Thank you for the quick reply. I just ran this updated pipeline. The parser element in between enc and dec was missing. I added queues before the videomixer inputs, but it doesn't seem to make a difference in the low framerate seen on the waylandsink.

    gst-launch-1.0 -v  videotestsrc ! video/x-raw, width=800, height=480, framerate=30/1 ! \
    ducatih264enc ! h264parse ! ducatih264dec ! \
    video/x-raw, format=NV12, framerate=30/1 ! vpe ! video/x-raw, format=RGB, framerate=30/1 ! \
    queue ! videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! \
    waylandsink sync=false \
    multifilesrc location="img.%04d.png" index=0 stop-index=1 loop=true caps="image/png,framerate=\(fraction\)30/1" ! pngdec ! videorate ! queue ! mix.

    I also noticed that the ducatih264dec seems to resize the height and width:

    /GstPipeline:pipeline0/GstH264Parse:h264parse0.GstPad:src: caps = "video/x-h264\,\ width\=\(int\)800\,\ height\=\(int\)480\,\ alignment\=\(string\)au\,\ stream-format\=\(string\)byte-stream\,....
    /GstPipeline:pipeline0/GstDucatiH264Dec:ducatih264dec0.GstPad:src: caps = "video/x-raw\,\ format\=\(string\)NV12\,\ width\=\(int\)896\,\ height\=\(int\)576\,\ framerate\=\(fraction\)30/1\,....

    If you could recommend specifically where to put the queue elements and caps that would be very helpful.

    Thanks,

    Vishal

  • Hello,

    Please add  height, width properties in the caps filters before and after vpe.

    You could add queues before the enc and dec.

    ...

    queue ! ducatih264enc ! h264parse ! queue ! ducatih264dec ! vpe ! video/x-raw, width=800, height=480, format=RGB, framerate=30/1 !

    ...

    It seems like you have made some changes in vpe element, right?

    I would recommend you to run the pipeline without the second branch (png decoding) and check the behavior on your side.

    BR

    Margarita

  • Hi Margarita,

    Yes I am using a VPE patch to enable RGB output that I obtained from another forum post.

    I ran the following pipeline but the output is still a low framerate:

    gst-launch-1.0 -v  videotestsrc ! video/x-raw, width=800, height=480, framerate=30/1 ! \
    queue ! ducatih264enc ! h264parse ! queue ! ducatih264dec ! \
    video/x-raw, width=896, height=576 ! vpe ! video/x-raw, width=800, height=480, format=RGB, framerate=30/1 ! \
    queue ! videomixer name=mix sink_0::alpha=1 ! \
    waylandsink sync=false
    

    I ran this with and without the height & width caps before the vpe - same result. The ducatih264dec didn't like 800x480 caps, so I had to set it to 896x576 as I mentioned before (not sure why this is the case).

    Is it possible to smoothly run videomixer for my usecase without the vpe colorspace conversion?

  • Hello,

    Could you try pipeline like:
    gst-launch-1.0 videomixer name=mixer ! videoconvert ! waylandsink sync=false videotestsrc ! video/x-raw, width=800, height=480, framerate=30/1 ! queue ! ducatih264enc ! h264parse ! queue ! ducatih264decvpe ! video/x-raw, width=800, height=480 ! queue ! mixer. videotestsrc pattern=13 ! "video/x-raw,format=AYUV,width=320,height=240,framerate=(fraction)10/1" ! queue ! mixer.

    You could check this e2e thread for examples with compositor element:
    e2e.ti.com/.../593312


    BR
    Margarita
  • Hi Margarita,

    Yes that runs, but it does not satisfy my latency requirements. When I try with my own encoded source from RTP (as opposed to the encoded videotestsrc), I get an increasing latency over time, on the order of 10s of seconds to even minutes. Is there a way to reduce this latency or at least keep it at a low fixed latency?

    Also, I noticed you mentioned in the other thread that glvideomixer is not available on AM5728, but is there another way to utilize the GPU for video mixing?

    I appreciate any resources or advice.

    Thanks,

    Vishal

  • Hello,

    Have you tried with the compositor element instead of videomixer?

    Could you try to increase num-buffers properties of vpe element also?

    Please set(increase the value of) the queue properties also.

    BR
    Margarita

  • Hi Margarita,

    Thanks for your reply.

    I have tried all your suggestions above, but the output video still has an increasing latency over time.

  • Hello,

    Vishal said:
    gst-launch-1.0 -v videotestsrc ! video/x-raw, width=800, height=480, framerate=30/1 ! \ queue ! ducatih264enc ! h264parse ! queue ! ducatih264dec ! \ video/x-raw, width=896, height=576 ! vpe ! video/x-raw, width=800, height=480, format=RGB, framerate=30/1 ! \ queue ! videomixer name=mix sink_0::alpha=1 ! \ waylandsink sync=false

    What will be your use case?

    Because in pipeline above you could remove encoder, parse, and decoder element. Something like:

    gst-launch-1.0 videomixer name=mixer ! videoconvert ! waylandsink videotestsrc pattern=snow ! "video/x-raw,format=AYUV,width=800,height=600,framerate=(fraction)30/1" ! queue ! mixer. videotestsrc pattern=13 ! "video/x-raw,format=AYUV,width=320,height=240,framerate=(fraction)10/1" ! queue ! mixer.

    BR
    Margarita

  • My use case involves an RTP video stream encoded in MJPEG (30 fps) which needs to be decoded and I need to overlay a buffer of PNGs on top of it at (~10 fps). The pipeline I've got working with a lot of latency looks like:

    gst-launch-1.0 -v videomixer name=mixer ! videoconvert ! waylandsink sync=false \
    udpsrc port=1234 caps="application/x-rtp, media=(string)video, payload=(int)26, clock-rate=(int)90000, ssrc=(guint)2823054885" ! rtpjitterbuffer ! rtpjpegdepay ! queue max-size-buffers=5000 ! decodebin ! vpe ! video/x-raw, width=800, height=480, format=NV12, framerate=30/1 ! queue max-size-buffers=5000 ! mixer. \
    videotestsrc pattern=1 ! video/x-raw, format=AYUV, width=320, height=240, framerate=10/1 ! queue max-size-buffers=5000 ! mixer.

    Except I would replace the second video branch with multifilesrc with PNGs which I've confirmed is working. This pipeline runs, but the latency seems to increase with time, which is not acceptable for my use case. In my use case I would also transcode the output of videomixer to h264 and then filesink, not waylandsink; I'm just using wayland sink so I can see the latency on the display. My final pipeline will look more like this (but even in this I am getting variable latency) :

    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, media=(string)video, payload=(int)26, clock-rate=(int)90000, ssrc=(guint)2823054885" ! rtpjitterbuffer ! rtpjpegdepay ! decodebin ! vpe ! \
    video/x-raw, format=RGB, width=800, height=480, framerate=30/1, interlace-mode=progressive, pixel-aspect-ratio=1/1 ! \
    videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! videoconvert ! \
    video/x-raw, format=NV12, width=800, height=480, framerate=30/1 ! \
    ducatih264enc ! filesink location=test_transcode.h264 sync=true \
    multifilesrc location="img.%04d.png" index=0 stop-index=1 loop=true caps="image/png,framerate=\(fraction\)10/1" ! pngdec ! videorate ! mix.

    Thanks

  • Hello,

    I would recommend you:
    1. add delay in the filesink element (ts-offset property). You could check the range of this property with gst-inspect command.
    2. disable synchronisation (sync=false).
    3. before the filesink please add ! queue max-size-bytes=65536 max-size-buffers=1000 max-size-time=0 leaky=downstream !...again with gst-inspect you could check the queue properties.
    4. add few more queues in the pipeline.
    5.add h264parse element after ducatih264enc (in other case the .h264 file could be corrupted).


    BR
    Margarita

  • Hi Margarita,

    Thanks for the suggestions. I tried the following pipeline:

    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, media=(string)video, payload=(int)26, clock-rate=(int)90000, ssrc=(guint)2823054885" ! rtpjitterbuffer ! rtpjpegdepay ! queue ! decodebin ! vpe ! \
    video/x-raw, format=RGB, width=800, height=480, framerate=30/1, interlace-mode=progressive, pixel-aspect-ratio=1/1 ! \
    videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! videoconvert ! \
    video/x-raw, format=NV12, width=800, height=480, framerate=30/1 ! \
    queue ! ducatih264enc ! h264parse ! queue max-size-bytes=65536 max-size-buffers=1000 max-size-time=0 leaky=downstream ! \
    filesink location=test_transcode.h264 ts-offset=-30000000000 sync=false \
    multifilesrc location="img.%04d.png" index=0 stop-index=1 loop=true caps="image/png,framerate=\(fraction\)2/1" ! pngdec ! videorate ! mix.

    It runs but the recorded video file still has latencies greater than 30-60 seconds, and it doesn't seem to be constant. I tried playing with the values of ts-offset (negative and positive) but it doesn't change much in the end result.

    To give more background context, the incoming RTP stream contains 1920x1080 MPEG video and the VPE is scaling down to 800x480. When I run this pipeline, the CPU usage is close to 100% between the two cores. I am assuming videomixer is utilizing the CPU for software rendering. Is this behavior typical for this use-case or should videomixer be able to handle with a lower fixed latency?

    Thank you,

    Vishal

  • Hello,

    Vishal said:
    It runs but the recorded video file still has latencies greater than 30-60 seconds, and it doesn't seem to be constant.

    It could be a network issue. Could you try to stream lower resolution

    Could you increase payload=96 and set encoding-name(recommended) ? 

    Vishal said:
    the incoming RTP stream contains 1920x1080 MPEG video

    I am confused what you are streaming mpeg or mjpeg or else?

    You could check with the top command the CPU load if it is higher the fps drop could be observe.

    Videomixer element is not a TI element, it is a open source element so I would recommend you to search over the internet about the usage etc.

    Vishal said:
    decodebin ! vpe ! \ video/x-raw, format=RGB, width=800, height=480, framerate=30/1, interlace-mode=progressive, pixel-aspect-ratio=1/1 ! \

    The format=RGB is it should be NV12 since the encoder requires NV12 format. I see that there is a videoconvert element which converts the output of the pngdec there is no point to convert the output of the decodebin to RGB and then to NV12.It should work if you set NV12 directly. This are additional mem copies.

    Per my understanding your usecase is video + png->mix->encode the both branches and save in file right?

    BR
    Margarita

  • Hi Margarita,

    1. Sorry about the confusion, the encoded video stream is in MJPEG. Also your understanding of the usecase is correct.

    2. I don't think it's a network issue because pipelines to wayland and filesink without videomixer work perfectly.

    3. The CPU usage as I mentioned earlier goes up to 100% between the 2 cores.

    4. I changed payload=96, but that doesn't work because JPEG encoding corresponds to 26.

    5. Originally I was using RGB because I wanted to avoid using videoconvert all-together to minimize CPU software rendering. I changed it back to NV12 as you suggested. The latency seems to be more reproducible now. However now I am noticing that after approx 40-50 seconds of recording, the PNG alternating still continues to record but the background camera feed is completely frozen. It normally stays frozen, but once I have seen it come back live. I tried adding queues before the videomixer sinks, but no effect. Any idea as to what is going on there? The pipeline I used is:

    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, media=(string)video, payload=(int)26, clock-rate=(int)90000, ssrc=(guint)2823054885" ! rtpjitterbuffer ! rtpjpegdepay ! queue ! decodebin ! vpe ! \
    video/x-raw, format=NV12, width=800, height=480, framerate=30/1 ! \
    videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! videoconvert ! \
    video/x-raw, format=NV12, width=800, height=480, framerate=30/1 ! \
    queue ! ducatih264enc ! h264parse ! queue max-size-bytes=65536 max-size-buffers=1000 max-size-time=0 leaky=downstream ! \
    filesink location=test_transcode.h264 ts-offset=30000000000 sync=false \
    multifilesrc location="img.%04d.png" index=0 stop-index=1 loop=true caps="image/png,framerate=\(fraction\)5/1" ! pngdec ! videorate ! mix.

    Thanks,

    Vishal

  • Hello,

    Vishal said:
    4. I changed payload=96, but that doesn't work because JPEG encoding corresponds to 26.

    For payload value >=96,  encoding-name should be set also. Here is example encoding-name=(string)JPEG.


    I see in the pipeline after the videorate element I do not see the caps filter. Here is example of videorate usage ...! videorate ! video/x-raw,framerate=5/1 ! ...

    Vishal said:
    , the PNG alternating still continues to record but the background camera feed is completely frozen. It normally stays frozen, but once I have seen it come back live

    I am not sure that I understand this.

    If you remove the png branch do you see this?

    Since the latency is reduced could you give a try when ts-offset=30000000000 is removed?

    BR
    Margarita

  • Hello,

    I am closing this thread.
    Please if it is still unresolved, reopen it again.

    BR
    Margarita
  • Hi Margarita,

    Apologies for the late reply. I tried your latest suggestions , but the issue I mentioned before still remains. What I meant last time is, the final output (h264 encoded mixed video stream) has some latency, but has a valid recording up until about 40-50 seconds, after which the camera stream is frozen but the png branch continues to swap through the buffer of pngs. So basically the rest of the video recording after 40-50 seconds, is a frozen camera stream with a swapping PNG overlay.

    Any suggestions as to why this may be happening? This freezing behaviour does not exist when I save the camera stream to h264 encoded to filesink directly (with no videomixer). Here is the pipeline I ran:

    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, media=(string)video, payload=(int)26, encoding-name=(string)JPEG, clock-rate=(int)90000, ssrc=(guint)2823054885" ! rtpjitterbuffer ! rtpjpegdepay ! queue ! decodebin ! vpe ! \
    video/x-raw, format=NV12, width=800, height=480, framerate=30/1 ! \
    videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! videoconvert ! \
    video/x-raw, format=NV12, width=800, height=480, framerate=30/1 ! \
    queue ! ducatih264enc ! h264parse ! queue max-size-bytes=65536 max-size-buffers=1000 max-size-time=0 leaky=downstream ! \
    filesink location=test_transcode.h264 ts-offset=30000000000 sync=false \
    multifilesrc location="img.%04d.png" index=0 stop-index=1 loop=true caps="image/png,framerate=\(fraction\)5/1" ! pngdec ! videorate ! video/x-raw,framerate=5/1 ! mix.

    Thanks,

  • Hello,

    Do you observe the hang in these cases?

    1.
    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, payload=(int)26, encoding-name=(string)JPEG" ! rtpjitterbuffer ! queue ! rtpjpegdepay ! queue ! jpegparse ! queue ! ducatijpegdecvpe ! video/x-raw, format=NV12, width=800, height=480 ! videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! videoconvert ! queue ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false multifilesrc location="img.%04d.png" index=0 stop-index=1 loop=true caps="image/png, framerate=\(fraction\)5/1" ! pngdec ! mix.

    2.
    If you replace the udpsrc with filesrc.

    BR
    Margarita
  • 1. When I try that pipeline, the final output video is all jumbled up with random colours, and while it runs I periodically get the message:

    invalid video buffer received
    WARNING: from element /GstPipeline:pipeline0/GstVideoConvert:videoconvert0: Internal GStreamer error: code not implemented.  Please file a bug at bugzilla.gnome.org/enter_bug.cgi.
    Additional debug info:
    ../../../../gst-plugins-base-1.8.3/gst-libs/gst/video/gstvideofilter.c(292): gst_video_filter_transform (): /GstPipeline:pipeline0/GstVideoConvert:videoconvert0:
    

    2. The pipeline does not work when I replace udpsrc with filesrc

  • Hello,

    Sorry I forgot the capsfilter after videoconvert element.
    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, payload=(int)26, encoding-name=(string)JPEG" ! rtpjitterbuffer ! queue ! rtpjpegdepay ! queue ! jpegparse ! queue ! ducatijpegdecvpe ! video/x-raw, format=NV12, width=800, height=480 ! videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! videoconvert ! video/x-raw, format=NV12, width=800, height=480 ! queue ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false multifilesrc location="img.%04d.png" index=0 stop-index=1 loop=true caps="image/png, framerate=\(fraction\)5/1" ! pngdec ! mix.

    BR
    Margarita
  • Hi Margarita,

    Thank you for the quick reply.

    I ran your updated pipeline, but the framerate was at 5 fps so I added a 30 fps cap at the videomixer sink (for camera feed). Again I am seeing the same issue of camera feed freezing as I described several times. However, by curiosity I scaled down the camera feed with the vpe to 400x240, and found that the latency was minimal and I did not see any freezing even after 2 minutes of recording. Do you suspect any thing that may cause this issue to be happening at the larger resolution and not at lower res? Could it have something to do with the limited CMA / CMEM buffer pools size?

    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, payload=(int)26, encoding-name=(string)JPEG" ! rtpjitterbuffer ! queue ! rtpjpegdepay ! queue ! jpegparse ! queue ! ducatijpegdecvpe ! video/x-raw, format=NV12, width=400, height=240, framerate=30/1 ! videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! videoconvert ! video/x-raw, format=NV12, width=400, height=240 ! queue ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false multifilesrc location="img.%04d.png" index=0 stop-index=1 loop=true caps="image/png, framerate=\(fraction\)5/1" ! pngdec ! mix.



    Thanks again,

  • Hello,

    The easy way to test this on your side is to replace vpe with videoscale.
    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, payload=(int)26, encoding-name=(string)JPEG" ! rtpjitterbuffer ! queue ! rtpjpegdepay ! queue ! jpegparse ! queue ! ducatijpegdec ! videoscale ! video/x-raw, format=NV12, width=400, height=240, framerate=30/1 ! videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! videoconvert ! video/x-raw, format=NV12, width=400, height=240 ! queue ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false multifilesrc location="img.%04d.png" index=0 stop-index=1 loop=true caps="image/png, framerate=\(fraction\)5/1" ! pngdec ! mix.

    If it is working you could increase cma.

    BR
    Margarita
  • Hi Margarita,

    There seem to be some caps missing in the pipeline you just sent. I'm getting a not-negotiated error. It shows from udpsrc, but I believe the issue is with ducatijpegdec, as I've encountered this before but was not sure what caps were missing:

    Setting pipeline to PAUSED ...
    /GstPipeline:pipeline0/GstMultiFileSrc:multifilesrc0.GstPad:src: caps = "image/png\,\ width\=\(int\)1\,\ height\=\(int\)1\,\ framerate\=\(fraction\)5/1\,\ pixel-aspect-ratio\=\(fraction\)1/1"
    /GstPipeline:pipeline0/GstPngDec:pngdec0.GstPad:sink: caps = "image/png\,\ width\=\(int\)1\,\ height\=\(int\)1\,\ framerate\=\(fraction\)5/1\,\ pixel-aspect-ratio\=\(fraction\)1/1"
    /GstPipeline:pipeline0/GstPngDec:pngdec0.GstPad:src: caps = "video/x-raw\,\ format\=\(string\)RGBA\,\ width\=\(int\)300\,\ height\=\(int\)300\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ colorimetry\=\(string\)sRGB\,\ framerate\=\(fraction\)5/1"
    Pipeline is live and does not need PREROLL ...
    /GstPipeline:pipeline0/GstVideoMixer2:mix.GstVideoMixer2Pad:sink_1: caps = "video/x-raw\,\ format\=\(string\)RGBA\,\ width\=\(int\)300\,\ height\=\(int\)300\,\ interlace-mode\=\(string\)progressive\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ colorimetry\=\(string\)sRGB\,\ framerate\=\(fraction\)5/1"
    Setting pipeline to PLAYING ...
    New clock: GstSystemClock
    /GstPipeline:pipeline0/GstUDPSrc:udpsrc0.GstPad:src: caps = "application/x-rtp\,\ payload\=\(int\)26\,\ encoding-name\=\(string\)JPEG\,\ media\=\(string\)video\,\ clock-rate\=\(int\)90000"
    /GstPipeline:pipeline0/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:sink: caps = "application/x-rtp\,\ payload\=\(int\)26\,\ encoding-name\=\(string\)JPEG\,\ media\=\(string\)video\,\ clock-rate\=\(int\)90000"
    /GstPipeline:pipeline0/GstRtpJitterBuffer:rtpjitterbuffer0.GstPad:sink: caps = "application/x-rtp\,\ payload\=\(int\)26\,\ encoding-name\=\(string\)JPEG\,\ media\=\(string\)video\,\ clock-rate\=\(int\)90000"
    /GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = "application/x-rtp\,\ payload\=\(int\)26\,\ encoding-name\=\(string\)JPEG\,\ media\=\(string\)video\,\ clock-rate\=\(int\)90000"
    /GstPipeline:pipeline0/GstQueue:queue0.GstPad:src: caps = "application/x-rtp\,\ payload\=\(int\)26\,\ encoding-name\=\(string\)JPEG\,\ media\=\(string\)video\,\ clock-rate\=\(int\)90000"
    /GstPipeline:pipeline0/GstRtpJPEGDepay:rtpjpegdepay0.GstPad:sink: caps = "application/x-rtp\,\ payload\=\(int\)26\,\ encoding-name\=\(string\)JPEG\,\ media\=\(string\)video\,\ clock-rate\=\(int\)90000"
    /GstPipeline:pipeline0/GstRtpJPEGDepay:rtpjpegdepay0.GstPad:src: caps = "image/jpeg\,\ framerate\=\(fraction\)0/1\,\ width\=\(int\)1920\,\ height\=\(int\)1080"
    /GstPipeline:pipeline0/GstQueue:queue1.GstPad:sink: caps = "image/jpeg\,\ framerate\=\(fraction\)0/1\,\ width\=\(int\)1920\,\ height\=\(int\)1080"
    /GstPipeline:pipeline0/GstQueue:queue1.GstPad:src: caps = "image/jpeg\,\ framerate\=\(fraction\)0/1\,\ width\=\(int\)1920\,\ height\=\(int\)1080"
    /GstPipeline:pipeline0/GstJpegParse:jpegparse0.GstPad:sink: caps = "image/jpeg\,\ framerate\=\(fraction\)0/1\,\ width\=\(int\)1920\,\ height\=\(int\)1080"
    /GstPipeline:pipeline0/GstJpegParse:jpegparse0.GstPad:src: caps = "image/jpeg\,\ parsed\=\(boolean\)true\,\ format\=\(string\)UYVY\,\ width\=\(int\)1920\,\ height\=\(int\)1080\,\ framerate\=\(fraction\)0/1"
    /GstPipeline:pipeline0/GstQueue:queue2.GstPad:sink: caps = "image/jpeg\,\ parsed\=\(boolean\)true\,\ format\=\(string\)UYVY\,\ width\=\(int\)1920\,\ height\=\(int\)1080\,\ framerate\=\(fraction\)0/1"
    /GstPipeline:pipeline0/GstQueue:queue2.GstPad:sink: caps = "image/jpeg\,\ parsed\=\(boolean\)true\,\ format\=\(string\)UYVY\,\ width\=\(int\)1920\,\ height\=\(int\)1080\,\ framerate\=\(fraction\)0/1"
    /GstPipeline:pipeline0/GstDucatiJpegDec:ducatijpegdec0.GstPad:src: caps = "video/x-raw\,\ format\=\(string\)NV12\,\ width\=\(int\)1920\,\ height\=\(int\)1088\,\ framerate\=\(fraction\)0/1\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ drm_mem\=\(boolean\)true"
    /GstPipeline:pipeline0/GstDucatiJpegDec:ducatijpegdec0.GstPad:sink: caps = "image/jpeg\,\ parsed\=\(boolean\)true\,\ format\=\(string\)UYVY\,\ width\=\(int\)1920\,\ height\=\(int\)1080\,\ framerate\=\(fraction\)0/1"
    /GstPipeline:pipeline0/GstDucatiJpegDec:ducatijpegdec0.GstPad:src: caps = "video/x-raw\,\ format\=\(string\)NV12\,\ width\=\(int\)1920\,\ height\=\(int\)1088\,\ framerate\=\(fraction\)0/1\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ drm_mem\=\(boolean\)true\,\ max-ref-frames\=\(int\)1"
    ERROR: from element /GstPipeline:pipeline0/GstUDPSrc:udpsrc0: Internal data flow error.
    Additional debug info:
    ../../../../gstreamer-1.8.3/libs/gst/base/gstbasesrc.c(2948): gst_base_src_loop (): /GstPipeline:pipeline0/GstUDPSrc:udpsrc0:
    streaming task paused, reason not-negotiated (-4)
    Execution ended after 0:00:00.297842901
    

    Thanks,

    Vishal

  • Hello,

    You should remove framerate in this caps:
    ! videoscale ! video/x-raw, format=NV12, width=400, height=240, framerate=30/1 !

    BR
    Margarita
  • Hi Margarita,

    I ran with the framerate removed with videoscale. It runs but again same issue of camera feed freezing after 40-50 seconds. But it's important to note that after 2 minutes of recording, the camera feed does unfreeze sometimes. Just not sure what is causing it to freeze to begin with, as the camera feed does not freeze in a regular recording (without videomixer).

    Could the queues be adjusted to accommodate this or is the pipeline simple running low on memory buffers?

    Thanks,
  • Hello,

    Since it freeze even with videoscale the problem is not in vpe.
    Probably there is a issue with videomixer.
    Could you try to add queue element before videomixer element to provide some more buffering(queue leaky=downstream)?

    You could try this also. The png branch is removed:

    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, payload=(int)26, encoding-name=(string)JPEG" ! rtpjitterbuffer ! queue ! rtpjpegdepay ! queue ! jpegparse ! queue ! ducatijpegdecvpe ! video/x-raw, format=NV12, width=400, height=240 ! videomixer name=mix ! queue ! videoconvert ! video/x-raw, format=NV12, width=400, height=240 ! queue ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false

    BR
    Margarita
  • Could you remove -v option also?

    BR
    Margarita
  • Hi Margarita,

    Thank you for the suggestions.

    Adding the queue leaky=downstream before the videomixer seemed to have increased the time it records before the freeze. Now it tends to freeze after about 80 seconds of recording.

    I tried the pipeline you provided without the png branch and that works fine without freezing.

    I also tried a pipeline with videomixer and instead of png branch I mixed in videotestsrc and that also gives similar results of freezing:

    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, payload=(int)26, encoding-name=(string)JPEG" ! rtpjitterbuffer ! queue ! rtpjpegdepay ! queue ! jpegparse ! queue ! ducatijpegdecvpe ! video/x-raw, format=NV12, width=800, height=480 ! queue leaky=downstream ! videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! queue ! videoconvert ! video/x-raw, format=NV12, width=800, height=480 ! queue ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false \
    videotestsrc pattern=1 ! \
    video/x-raw,format=ARGB,framerate=\(fraction\)30/1,width=200,height=200 ! mix.

    Is there an alternative option to obtain this video mixing, ultilizing the hardware blocks or GPU acceleration on AM5728?

    Thanks again,

    Vishal

  • Hello,

    I ran this pipeline on my side for ~14 mins, the hang/freeze on display was not observed.
    root@am57xx-evm:~# gst-launch-1.0 compositor name=mix ! queue ! videoconvert ! waylandsink sync=false videotestsrc ! video/x-raw, format=NV12, width=1280, height=720, framerate=30/1 ! queue ! ducatijpegenc ! jpegparse ! queue ! ducatijpegdecvpe ! 'video/x-raw, format=(string)NV12, width=(int)800, height=(int)480' ! mix. videotestsrc pattern=18 ! 'video/x-raw, format=(string)AYUV,framerate=(fraction)5/1, width=(int)200, height=(int)200' ! mix.
    Setting pipeline to PAUSED ...
    [ 96.563776] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
    Pipeline is PREROLLING ...
    Redistribute latency...
    Pipeline is PREROLLED ...
    Setting pipeline to PLAYING ...
    New clock: GstSystemClock
    ^Chandling interrupt.
    Interrupt: Stopping pipeline ...
    Execution ended after 0:14:53.091689053
    Setting pipeline to PAUSED ...
    Setting pipeline to READY ...
    Setting pipeline to NULL ...
    Freeing pipeline ...
    root@am57xx-evm:~#

    BR
    Margarita
  • Hi Margarita,

    I ran the pipeline you sent and it works fine on my side as well. In order to adapt to my use case, I changed it to the following and tried:

    gst-launch-1.0 compositor name=mix ! queue ! videoconvert ! video/x-raw, format=NV12, width=800, height=480 ! queue ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false udpsrc port=1234 caps="application/x-rtp, payload=(int)26, encoding-name=(string)JPEG" ! rtpjitterbuffer ! queue ! rtpjpegdepay ! queue ! jpegparse ! queue ! ducatijpegdecvpe ! 'video/x-raw, format=(string)NV12, width=(int)800, height=(int)480' ! mix. videotestsrc pattern=18 ! 'video/x-raw, format=(string)AYUV,framerate=(fraction)30/1, width=(int)200, height=(int)200' ! mix.

    Again, it results in the same problem of freezing after 40 seconds or so. I also tried a waylandsink variant (instead of ducatih264enc --> filesink) of the above pipeline, and it also freezes after a minute or so of recording. Notice that I had to increase the framerate of the videotestsrc to 30/1. When I left it at 5/1, the camera feed was also recorded at 5/1. I tried to add caps after the camera feed to fix it to 30/1, but I was not successful. I tried adding framerate caps in the udpsrc caps as well as after ducatijpegdecvpe. Example:

    gst-launch-1.0 compositor name=mix ! queue ! videoconvert ! video/x-raw, format=NV12, width=800, height=480 ! queue ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false udpsrc port=1234 caps="application/x-rtp, payload=(int)26, encoding-name=(string)JPEG" ! rtpjitterbuffer ! queue ! rtpjpegdepay ! queue ! jpegparse ! queue ! ducatijpegdecvpe ! 'video/x-raw, format=(string)NV12, width=(int)800, height=(int)480, framerate=(fraction)30/1' ! mix. videotestsrc pattern=18 ! 'video/x-raw, format=(string)AYUV,framerate=(fraction)5/1, width=(int)200, height=(int)200' ! mix.

    Results in :

    Setting pipeline to PAUSED ...
    Pipeline is live and does not need PREROLL ...
    Setting pipeline to PLAYING ...
    New clock: GstSystemClock
    Redistribute latency...
    Redistribute latency...
    **
    ERROR:gstducatividenc.c:426:gst_ducati_videnc_configure: assertion failed: (self->output_pool == NULL)
    Aborted (core dumped)
    

    What is the proper way of setting the framerate of the udpsrc camera stream, so that videomixer/compositor has a consistent 30 fps at it's sink?

    Thanks,

    Vishal

  • Hello Vishal,

    Could you  remove rtpjitterbuffer element in the pipeline with videomixer element?

    BR
    Margarita

  • Hi Margarita,

    I tried the following pipeline without rtpjitterbuffer

    gst-launch-1.0 -v udpsrc port=1234 caps="application/x-rtp, payload=(int)26, encoding-name=(string)JPEG" ! queue ! rtpjpegdepay ! queue ! jpegparse ! queue ! ducatijpegdecvpe ! video/x-raw, format=NV12, width=800, height=480 ! queue leaky=downstream ! videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! queue ! videoconvert ! video/x-raw, format=NV12, width=800, height=480 ! queue ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false \
    videotestsrc pattern=1 ! \
    video/x-raw,format=ARGB,framerate=\(fraction\)30/1,width=200,height=200 ! mix.

    Same freezing problem.

    Thanks,

  • Hello,

    Please when you try remove -v option.
    What is PSDK version that you are using?
    Videomixer element is not a TI element.
    Could you try leaky=upstream also.

    BR
    Margarita
  • I tried without -v and with leaky=upstream. Same results.

    I believe I am using PSDK 4.00.00.04.

    Thanks,
  • Hello,

    I tried this pipeline. The pipeline has 2 encoders and one decoder:

    gst-launch-1.0 -v videotestsrc ! video/x-raw, format=NV12, width=1280, height=720, framerate=30/1 ! queue ! ducatijpegenc ! jpegparse ! queue ! ducatijpegdec ! vpe num-input-buffers=8 ! 'video/x-raw, format=(string)NV12, width=(int)800, height=(int)480' ! queue leaky=downstream ! videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! queue ! videoconvert ! video/x-raw, format=NV12, width=800, height=480 ! queue ! vpe ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false videotestsrc pattern=1 ! video/x-raw,format=ARGB,framerate=\(fraction\)30/1,width=200,height=200 ! mix.

    I do not observe hang.
    gst-launch-1.0 playbin uri=file:///home/root/test_transcode.h264 video-sink=waylandsink
    Setting pipeline to PAUSED ...
    Pipeline is PREROLLING ...
    Pipeline is PREROLLED ...
    Setting pipeline to PLAYING ...
    New clock: GstSystemClock
    Got EOS from element "playbin0".
    Execution ended after 0:05:35.088471749
    Setting pipeline to PAUSED ...
    Setting pipeline to READY ...
    Setting pipeline to NULL ...
    Freeing pipeline ...

    Except the additional encoder (to provide mjpeg video) there is additional vpe element. The vpe's property num-input-buffers is also set. I tried same but with compositor element the result is the same.
    Did you try to increase this udpsrc's property buffer-size ?
    You could try to replace udpsrc with rtspsrc element if it fit your use case.

    BR
    Margarita
  • Hello Vishal,

    Did you have a chance to try the latest suggestions?
    Is it working now?

    BR
    Margarita
  • Hi Margarita,

    Thanks for the follow-up.

    The pipeline you provided runs successfully without freezing. When I change the videotestsrc branch to my udpsrc branch the same problem of freezing after 1 minute of recording occurs. I tried increasing the buffer-size property of udpsrc as well like:

    gst-launch-1.0 udpsrc buffer-size=2147483647 port=1234 caps="application/x-rtp, payload=(int)26, encoding-name=(string)JPEG" ! rtpjitterbuffer ! queue ! rtpjpegdepay ! queue ! jpegparse ! queue ! ducatijpegdec ! vpe num-input-buffers=8 ! video/x-raw, format=NV12, width=800, height=480 ! queue leaky=downstream ! videomixer name=mix sink_0::alpha=1 sink_1::alpha=0.7 ! queue ! videoconvert ! video/x-raw, format=NV12, width=800, height=480 ! queue ! vpe ! ducatih264enc ! h264parse ! queue ! filesink location=test_transcode.h264 sync=false videotestsrc pattern=1 ! video/x-raw,format=ARGB,framerate=\(fraction\)30/1,width=200,height=200 ! mix.

    While its running the CPU usage is typically around 130 %, and I've seen memory usage start around 200 MiB and increase above 360 MiB as the recording continues. I have yet to try replacing udpsrc to rtpsrc.

    It seems to me that using videomixer for my application is probably not the best way to go considering it does not utilize the GPU for video mixing. My end goal is to get QT generated content overlayed on-top of a live camera stream within gstreamer so that it can be recorded (encoded and saved to file). I'm currently looking into other options revolving around EGLImage. If you have any other suggestions, please point me in the right direction.


    Thanks again for your support,

    Vishal

  • Hello,

    I am sorry but I am not aware with QT.
    It is normal to observe high CPU load with videomixer element. Compositor element could be used also but the CPU load will be higher again.

    BR
    Margarita
  • Hello Vishal,

    I will close this thread, please for QT questions open a new topic.

    BR
    Margarita
  • Hi Margarita,

    Before you close the thread. Do you know of any gstreamer plugins (open source or TI) that allow for hardware accelerated (GPU/video hardware) video or text overlay?

    Thanks,
    Vishal
  • Hello,

    If you mean something like compositor or videomixer TI does not have such plugin.
    You could check TI multimedia user guide:
    processors.wiki.ti.com/.../Processor_Training:_Multimedia
    Elements like textoverlay, videomixer, compositor are running on A15.

    BR
    Margarita
  • fwiw, I have had the same problem with rstpsrc using gst-launch-0.10. The machine could not keep up with the incoming framerate and was buffering all the unprocessed frames until the memory limit was reached. I solved it by adding "is-live=true" to the source, and changing my queue to "queue leaky=1 max-size-time=25000".
    I am not aware of any GPU-based mixer/overlay plug-ins.
    I have also had issues with videotestsrc using up tons of CPU time.
  • Hello,

    This thread has been closed. Please open a new e2e topic. Provide information about PSDK version that you are using etc.

    BR
    Margarita