This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BEAGLEBK: eHRPWM independent channels

Part Number: BEAGLEBK

I'd like to use the EHRPWM2 for 2 independent signals - 2A; would run @ 1kHz with a varying duty-cycle, while 2B would run @ 10kHz with a varying duty-cycle.

Is this possible?

[background]

I couldn't tell from the manual if the A & B channels use the same clock source (which, as I understand it, define the frequency of the signal).