This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4378: MMC2 WiFi bring-up

Part Number: AM4378

Tool/software: Linux

Hi

I am trying to bring up the wifi on AM4378 processor based board. I am using dtb and Linux kernel which is built from ti-processor-sdk-linux-am437x-evm-04.00.00.04

wifi module (WF111 from Silicon Labs) is connected to mmc2 pins of AM4378 over SDIO interface using TXS026 (SDIO Port Extender).  In the below table i have specified the pin connections between AM437, TXS026 and WF111. TXS026 SEL pin is connected to GND to select B0.

AM437   TXS026   WF111
Ball Num Mode 3 input output  
AD21 MMC2_CLK CLKA CLKB0 SDIO_CLK
AE22 MMC2_CMD CMDA CMDB0 SDIO_CMD
AD22 MMC2_DAT0 DATA0A DATA0B0 SDIO_DATA0
AE23 MMC2_DAT1 DATA1A DATA1B0 SDIO_DATA1
AD23 MMC2_DAT2 DATA2A DATA2B0 SDIO_DATA2
AE24 MMC2_DAT3 DATA3A DATA3B0 SDIO_DATA3

Please can you tell me what  changes should i do in device tree or kernel build process to bring the wifi up.

Thanks