Part Number: BEAGLEBK
Other Parts Discussed in Thread: DAC7512, PMP, TCA6416, TCA8418, LM8323, LM8333, ADS7846, TSC2004, TSC2005, TSC2007, TPS65218, TWL6040, PCF8574, DRV2665, DRV2667, TPIC2810, TPS65910, BQ27000, LP8727, BQ24190, BQ24257, BQ24735, BQ25890, TPS65090, TPS65217, LM63, LM70, LM73, LM77, LM80, LM83, LM87, LM90, LM92, LM93, LM95234, LM95241, LM95245, ADC128D818, ADS1015, ADS7828, ADS7871, AMC6821, INA209, INA3221, TMP102, TMP103, TMP401, TMP421, LP3943, TPS65010, TPS65086, TPS65912, LM3533, LP3971, LP3972, TPS51632, TPS62360, TPS65023, TLV320AIC23B, TVP5150, TVP7002, THS8200, LM3560, THS7303, OPA362, TFP410, TPD12S015, DA8XX, LM3630A, LM3639, PCM1681, PCM3168A, TAS2552, TAS5086, TS3A227E, TPA6130A2, LM3530, LM3642, LP3944, LP5521, LP5523, LP5562, LP8501, DAC124S085, TCA6507, CDCE706, CDCE925, ADC128S052, ADC161S626, ADS8688, AFE4403, AFE4404, OPT3001, TMP006
Tool/software: Linux
Hello,
did follow exactly the description 
Status:
1.) AD activated in kernel as described ... make zImage copy zImage into /boot ... ok
2.) make modules and make install_modules ..... verified, ok
3.) append the described devicetree stuff to arch/arm/boot/dts/am335x-boneblack.dts , make make am335x-boneblack.dtb copy arch/arm/boot/dts/am335x-boneblack.dtb into /boot
&tscadc {
adc {
ti,adc-channels = <4 5 6 7>;
};
};
4.) reboot, lsmod did not list ti_am335x_adc
after modprobe ti_am335x_adc it's there
lsmod | grep ti_am
ti_am335x_adc 6837 0
ti_am335x_tscadc 6162 1 ti_am335x_adc
5.) but I can't see the devices
ls -al /sys/bus/iio/devices/iio\:device0/
ls: /sys/bus/iio/devices/iio:device0/: No such file or directory
ls -al /sys/bus/iio/devices/
drwxr-xr-x 2 root root 0 Mar 26 15:17 .
drwxr-xr-x 4 root root 0 Mar 26 15:17 .
What is missing?