Part Number: AM3352
Other Parts Discussed in Thread: AM4379
Hello Champs,
Customer connected 4GB emmc (compatible to 4.5.1) to mmc0 and connected SD card to MMC1. The boot procedure is MMC1->MMC0.
1. Board can boot from SD card and enter Uboot, he can use mmc command to read the EMMC correctly.
2. EMMC Linux partition: Partition1 FAT32: MLO, uboot.img, uboot.env;
Partition2 EXT4: rootfs.
3. Remove sd card, re-power the board and there is no output from serial port, the voltage has no change.
Uboot uses am335x_evm_defconfig.
Thanks.
Rgds
Shine