This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: AM3354BZCZA100 questions

Part Number: AM3354

Hi,all

      I have some questions about AM3354BZCZA100, please help me check them, thanks.

     1. What time is the mass production of AM3354BZCZA100?

     2. How many is the device production by year?

     3. What main applications are the device used to?

     4. Which main regions are the device sell to?

     5. How many is the device sell to China?

     6. Can the device support to android system and WinCE system?

     7. Are there peripheral modes supported by the AM3354BZCZA100? Like WIFI,BT,Zigbee mode are general, not must be customized.

     8. Is there any upgrade device for AM3354BZCZA100? Which one?

     9. AM3354BZCZA100 will be stop production? How long will be production? Can be five years,or more?

     

     Thank a lot

      

  • The factory team have been notified. They will respond here.
  • Hi,Biser
    Thank you.
    When will reply by expected? Because the customer want to change the AM3354 by other manufacturers.
  • Went,
    Thanks for your patience. Posts normally are replied within a period of 24 hours, in some case takes more time depending on the issue.
    See comments below:

    1. What time is the mass production of AM3354BZCZA100?
    TI: AM3354 is in mass production now. It still did not reach its peak production since we see its volume increasing year over year.

    2. How many is the device production by year?
    TI: AM335x is sold in Millions of devices per year.

    3. What main applications are the device used to?
    TI: AM335x is a broad market device, we sell it to all kind of markets.

    4. Which main regions are the device sell to?
    TI: It is sold to all regions of the world. As mentioned before, it is a broad market device with customers everywhere.

    5. How many is the device sell to China?
    TI: Millions. We do not open specifics.

    6. Can the device support to android system and WinCE system?
    TI: Yes. via 3P. Check this link: www.ti.com/.../companyfolder.tsp

    7. Are there peripheral modes supported by the AM3354BZCZA100? Like WIFI,BT,Zigbee mode are general, not must be customized.
    TI: yes. Please check: www.ti.com/.../PROCESSOR-SDK-AM335X

    8. Is there any upgrade device for AM3354BZCZA100? Which one?
    TI: we offer a large range of processors, with higher or lower performance than AM3354. I recommend to you to check this address: www.ti.com/.../overview.html
    Depending on what you need, we have different options for you.

    9. AM3354BZCZA100 will be stop production? How long will be production? Can be five years,or more?
    TI: see comment to question #1. We have no EOL plans at this time.
  • Hi,Rogerio

    1. What time is the mass production of AM3354BZCZA100?
    TI: AM3354 is in mass production now. It still did not reach its peak production since we see its volume increasing year over year.
    Went:Sorry for that, I want to know when be producted the device? 2012? or 2013?
    3. What main applications are the device used to?
    TI: AM335x is a broad market device, we sell it to all kind of markets.
    Went: Could you tell me the main applications are what? Like test measure or others, The main.
    4. Which main regions are the device sell to?
    TI: It is sold to all regions of the world. As mentioned before, it is a broad market device with customers everywhere.
    Went: I want to know the main regions, like USA or others.

    Thanks a lot
  • Went,
    1) 2012
    3) It is impossible to track all applications where this device is used, since it is a broad market device and there are thousands of designs that we were not involved. I can tell you that Industrial is a major market for it.
    4) we do not break down numbers/revenue by region. We sell it WW.
  • Hi,Rogerio
    4. What is WW?
  • Went,
    WW means world wide.