This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3358: OpenSSL update in Yocto

Part Number: AM3358


Tool/software: Linux

Hi,

We are currently using Krogoth build (Yocto). We have to update openssl from 1.0.2h to 1.0.2o. For this, we have copied the recipe for openssl-1.0.2o from Rocko build (Yocto). When we are trying to compile we are getting the error/s as described below.

$ bitbake openssl

NOTE: Started PRServer with DBfile: /home/einfochips/project/tms/SEM3_UCM/build/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 45721, PID: 13109
Loading cache: 100% |####################################################################################################################################| ETA: 00:00:00
Loaded 2859 entries from dependency cache.
WARNING: /home/einfochips/project/tms/SEM3_UCM/sources/oe-core/meta/recipes-connectivity/openssl/openssl_1.0.2o.bb: Exception during build_dependencies for do_install-:--:--
WARNING: /home/einfochips/project/tms/SEM3_UCM/sources/oe-core/meta/recipes-connectivity/openssl/openssl_1.0.2o.bb: Error during finalise of /home/einfochips/project/tms/SEM3_UCM/sources/oe-core/meta/recipes-connectivity/openssl/openssl_1.0.2o.bb
ERROR: ExpansionError during parsing /home/einfochips/project/tms/SEM3_UCM/sources/oe-core/meta/recipes-connectivity/openssl/openssl_1.0.2o.bb: Failure expanding variable do_install, expression was # Create /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image//usr to fix parallel issues
mkdir -p /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image//usr/

oe_runmake INSTALL_PREFIX="/home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image" MANDIR="/usr/share/man" install

oe_libinstall -so libcrypto /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib
oe_libinstall -so libssl /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib

install -d /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/include
cp --dereference -R include/openssl /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/include

install -Dm 0755 /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/openssl-c_rehash.sh /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/bin/c_rehash
sed -i -e 's,/etc/openssl,/etc/ssl,g' /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/bin/c_rehash

oe_multilib_header openssl/opensslconf.h
if [ "${@bb.utils.filter('PACKAGECONFIG', 'perl', d)}" ]; then
sed -i -e '1s,.*,#!/usr/bin/env perl,' /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib/ssl/misc/CA.pl
sed -i -e '1s,.*,#!/usr/bin/env perl,' /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib/ssl/misc/tsget
else
rm -f /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib/ssl/misc/CA.pl /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib/ssl/misc/tsget
fi

# Create SSL structure
install -d /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/etc/ssl/
mv /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib/ssl/openssl.cnf \
/home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib/ssl/certs \
/home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib/ssl/private \
\
/home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/etc/ssl/
ln -sf /etc/ssl/certs /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib/ssl/certs
ln -sf /etc/ssl/private /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib/ssl/private
ln -sf /etc/ssl/openssl.cnf /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/lib/ssl/openssl.cnf

# Rename man pages to prefix openssl10-*
for f in `find /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/share/man -type f`; do
mv $f $(dirname $f)/openssl10-$(basename $f)
done
for f in `find /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0.arago0/image/usr/share/man -type l`; do
ln_f=`readlink $f`
rm -f $f
ln -s openssl10-$ln_f $(dirname $f)/openssl10-$(basename $f)
done
which triggered exception AttributeError: 'module' object has no attribute 'filter'

Summary: There were 2 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

We have followed this link as a reference for updating to openssl-1.0.2o version and resolving its relevant dependencies. Please help.

Regards,

Sunny.

  • Hello Sunny,

    You need to apply this patch.

    Best regards,
    Kemal

  • Hi,

    Applied the patch you suggested, but am still getting the same error.

    [PATCH]

    $ git diff bitbake/lib/bb/utils.py

    diff --git a/sources/bitbake/lib/bb/utils.py b/sources/bitbake/lib/bb/utils.py

    index 3544bbe..a6fe93b 100644

    --- a/sources/bitbake/lib/bb/utils.py

    +++ b/sources/bitbake/lib/bb/utils.py

    @@ -967,6 +967,26 @@ def contains_any(variable, checkvalues, truevalue, falsevalue, d):

            return truevalue

        return falsevalue

    +def filter(variable, checkvalues, d):

    +    """Return all words in the variable that are present in the checkvalues.

    +     Arguments:

    +     variable -- the variable name. This will be fetched and expanded (using

    +    d.getVar(variable)) and then split into a set().

    +     checkvalues -- if this is a string it is split on whitespace into a set(),

    +    otherwise coerced directly into a set().

    +     d -- the data store.

    +    """

    +    val = d.getVar(variable)

    +    if not val:

    +        return ''

    +    val = set(val.split())

    +    if isinstance(checkvalues, str):

    +        checkvalues = set(checkvalues.split())

    +    else:

    +        checkvalues = set(checkvalues)

    +    return ' '.join(sorted(checkvalues & val))

    +

    +

    def cpu_count():

        return multiprocessing.cpu_count()

    ------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

    [ERROR]

    $ bitbake openssl

    NOTE: Started PRServer with DBfile: /home/einfochips/project/tms/SEM3_UCM/build/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 45467, PID: 17905

    Loading cache: 100% |####################################################################################################################################| ETA:  00:00:00

    Loaded 2859 entries from dependency cache.

    WARNING: /home/einfochips/project/tms/SEM3_UCM/sources/oe-core/meta/recipes-connectivity/openssl/openssl_1.0.2o.bb: Exception during build_dependencies for do_install-:--:--

    WARNING: /home/einfochips/project/tms/SEM3_UCM/sources/oe-core/meta/recipes-connectivity/openssl/openssl_1.0.2o.bb: Error during finalise of /home/einfochips/project/tms/SEM3_UCM/sources/oe-core/meta/recipes-connectivity/openssl/openssl_1.0.2o.bb

    ERROR: ExpansionError during parsing /home/einfochips/project/tms/SEM3_UCM/sources/oe-core/meta/recipes-connectivity/openssl/openssl_1.0.2o.bb: Failure expanding variable do_install, expression was # Create /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image//usr to fix parallel issues

    mkdir -p /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image//usr/

    oe_runmake INSTALL_PREFIX="/home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image" MANDIR="/usr/share/man" install

    oe_libinstall -so libcrypto /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib

    oe_libinstall -so libssl /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib

    install -d /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/include

    cp --dereference -R include/openssl /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/include

    install -Dm 0755 /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/openssl-c_rehash.sh /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/bin/c_rehash

    sed -i -e 's,/etc/openssl,/etc/ssl,g' /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/bin/c_rehash

    oe_multilib_header openssl/opensslconf.h

    if [ "${@bb.utils.filter('PACKAGECONFIG', 'perl', d)}" ]; then

    sed -i -e '1s,.*,#!/usr/bin/env perl,' /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib/ssl/misc/CA.pl

    sed -i -e '1s,.*,#!/usr/bin/env perl,' /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib/ssl/misc/tsget

    else

    rm -f /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib/ssl/misc/CA.pl /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib/ssl/misc/tsget

    fi

    # Create SSL structure

    install -d /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/etc/ssl/

    mv /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib/ssl/openssl.cnf \

      /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib/ssl/certs \

      /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib/ssl/private \

      \

      /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/etc/ssl/

    ln -sf /etc/ssl/certs /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib/ssl/certs

    ln -sf /etc/ssl/private /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib/ssl/private

    ln -sf /etc/ssl/openssl.cnf /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/lib/ssl/openssl.cnf

    # Rename man pages to prefix openssl10-*

    for f in `find /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/share/man -type f`; do

       mv $f $(dirname $f)/openssl10-$(basename $f)

    done

    for f in `find /home/einfochips/project/tms/SEM3_UCM/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/openssl/1.0.2o-r0.arago0/image/usr/share/man -type l`; do

       ln_f=`readlink $f`

       rm -f $f

       ln -s openssl10-$ln_f $(dirname $f)/openssl10-$(basename $f)

    done

    which triggered exception TypeError: getVar() takes at least 3 arguments (2 given)

    Summary: There were 2 WARNING messages shown.

    Summary: There was 1 ERROR message shown, returning a non-zero exit code.

    ------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

    [openssl directory and its content is copied from Rocko version to Krogoth version]

    NOTE: We have removed the openssl  directory of Krogoth version and then replaced the whole directory and its content with openssl directory from the Rocko version.

    $ tree openssl/
    openssl/
    ├── openssl
    │   ├── 0001-Take-linking-flags-from-LDFLAGS-env-var.patch
    │   ├── openssl-c_rehash.sh
    │   └── run-ptest
    ├── openssl-1.0.2o
    │   ├── 0001-Fix-build-with-clang-using-external-assembler.patch
    │   ├── 0001-openssl-force-soft-link-to-avoid-rare-race.patch
    │   ├── configure-musl-target.patch
    │   ├── configure-targets.patch
    │   ├── debian
    │   │   ├── ca.patch
    │   │   ├── c_rehash-compat.patch
    │   │   ├── debian-targets.patch
    │   │   ├── man-dir.patch
    │   │   ├── man-section.patch
    │   │   ├── no-rpath.patch
    │   │   ├── no-symbolic.patch
    │   │   └── pic.patch
    │   ├── debian1.0.2
    │   │   ├── block_digicert_malaysia.patch
    │   │   ├── block_diginotar.patch
    │   │   ├── soname.patch
    │   │   └── version-script.patch
    │   ├── engines-install-in-libdir-ssl.patch
    │   ├── find.pl
    │   ├── Makefiles-ptest.patch
    │   ├── oe-ldflags.patch
    │   ├── openssl-c_rehash.sh
    │   ├── openssl-fix-des.pod-error.patch
    │   ├── openssl_fix_for_x32.patch
    │   ├── openssl-util-perlpath.pl-cwd.patch
    │   ├── parallel.patch
    │   ├── ptest-deps.patch
    │   ├── ptest_makefile_deps.patch
    │   ├── reproducible-cflags.patch
    │   ├── reproducible-mkbuildinf.patch
    │   ├── run-ptest
    │   ├── shared-libs.patch
    │   └── Use-SHA256-not-MD5-as-default-digest.patch
    ├── openssl_1.0.2o.bb
    ├── openssl10.inc
    └── openssl_1.1.0h.bb

    Regards,

    Sunny.

     

  • It is not the same error. Last time you was geting AttributeError: 'module' object has no attribute 'filter', now you get TypeError: getVar() takes at least 3 arguments (2 given). To fix this pass a "True" string to a getVar as a third argument since you are using the old API but the patch you apply and the new recipe you copy uses the new API.
    val = d.getVar(variable, True)

  • Oh, I see the difference in the error now. Thanks your answers solved the issue.

    Am a bit naive in using Yocto. To recapitulate, I followed the steps mentioned below to integrate openssl-1.0.2o from Rocko to Krogoth. Let me know if anything else needs to be taken care of. 

    1. Deleted openssl directory currently existing in the Krogoth source under "<source>/oe-core/meta/recipes-connectivity" folder.
    2. Copied openssl directory from Rocko to Krogoth under "<source>/oe-core/meta/recipes-connectivity" folder.
    3. Added openssl_%.bbappend file under "./meta-arago/meta-arago-distro/recipes-connectivity/openssl/" directory of Krogoth source.
    4. Added manpages.bbclass and relative_symlinks.bbclass from Rocko to Krogoth under "<source>/oe-core/meta/classes/" folder.
    5. Patch the Krogoth source with this patch.
    6. Changed val = d.getVar(variable) to val = d.getVar(variable, True) in the patched code as described in step 5.
    7. Patch the Krogoth source with this patch to overcome error "Exception: AttributeError: 'module' object has no attribute 'replace_absolute_symlinks'"
    8. Changed d.getVar('D') to d.getVar('D', True) in the relative_symlinks.bbclass under "<source>/oe-core/meta/classes/" folder.
    9. Removed openssl_1.1.0h.bb in Krogoth source from "<source>/oe-core/meta/recipes-connectivity/openssl/" folder
    10. Removed openssl_1.0.2h.bbappend in Krogoth source from "<source>/meta-arago/meta-arago-distro/recipes-connectivity/openssl/" folder.
    11. Applied the following commands and it compiled successfully.

    $ bitbake openssl -c cleansstate


    NOTE: Started PRServer with DBfile: /home/einfochips/project/tms/SEM3_UCM/build/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 35043, PID: 19786
    Loading cache: 100% |####################################################################################################################################| ETA: 00:00:00
    Loaded 2865 entries from dependency cache.
    Parsing recipes: 100% |##################################################################################################################################| Time: 00:00:00
    Parsing of 2263 .bb files complete (2262 cached, 1 parsed). 2859 targets, 474 skipped, 0 masked, 0 errors.
    NOTE: Resolving any missing task queue dependencies

    Build Configuration:
    BB_VERSION = "1.30.0"
    BUILD_SYS = "x86_64-linux"
    NATIVELSBSTRING = "Ubuntu-16.04"
    TARGET_SYS = "arm-linux-gnueabi"
    MACHINE = "am335x-evm"
    DISTRO = "arago"
    DISTRO_VERSION = "2016.12"
    TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
    TARGET_FPU = "hard"
    meta-arago-distro
    meta-arago-extras
    meta-qt5
    meta-networking
    meta-ruby
    meta-python
    meta-oe
    meta-ti
    meta-linaro-toolchain
    meta-optee
    meta
    meta-sem3 = "24VDC_dev:517ecbb4d9c5c872b6db726337a780c950ebf92f"

    NOTE: Preparing RunQueue
    NOTE: Executing RunQueue Tasks
    NOTE: Tasks Summary: Attempted 2 tasks of which 0 didn't need to be rerun and all succeeded.
    NOTE: Writing buildhistory

    $ bitbake openssl

    NOTE: Started PRServer with DBfile: /home/einfochips/project/tms/SEM3_UCM/build/cache/prserv.sqlite3, IP: 127.0.0.1, PORT: 35309, PID: 7178
    Loading cache: 100% |####################################################################################################################################| ETA: 00:00:00
    Loaded 2865 entries from dependency cache.
    Parsing recipes: 100% |##################################################################################################################################| Time: 00:00:00
    Parsing of 2263 .bb files complete (2261 cached, 2 parsed). 2859 targets, 474 skipped, 0 masked, 0 errors.
    NOTE: Resolving any missing task queue dependencies

    Build Configuration:
    BB_VERSION = "1.30.0"
    BUILD_SYS = "x86_64-linux"
    NATIVELSBSTRING = "Ubuntu-16.04"
    TARGET_SYS = "arm-linux-gnueabi"
    MACHINE = "am335x-evm"
    DISTRO = "arago"
    DISTRO_VERSION = "2016.12"
    TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
    TARGET_FPU = "hard"
    meta-arago-distro
    meta-arago-extras
    meta-qt5
    meta-networking
    meta-ruby
    meta-python
    meta-oe
    meta-ti
    meta-linaro-toolchain
    meta-optee
    meta
    meta-sem3 = "24VDC_dev:517ecbb4d9c5c872b6db726337a780c950ebf92f"

    NOTE: Preparing RunQueue
    NOTE: Executing SetScene Tasks
    NOTE: Executing RunQueue Tasks
    WARNING: external-linaro-toolchain-2016.11-r0.arago32 do_package: QA Issue: external-linaro-toolchain: Files/directories were installed but not shipped in any package:
    /lib/libgfortran.spec
    /lib/libsanitizer.spec
    /usr/sbin
    Please set FILES such that these items are packaged. Alternatively if they are unneeded, avoid installing them or delete them within do_install.
    external-linaro-toolchain: 3 installed and not shipped files. [installed-vs-shipped]
    NOTE: Tasks Summary: Attempted 431 tasks of which 389 didn't need to be rerun and all succeeded.
    NOTE: Writing buildhistory

    Summary: There was 1 WARNING message shown.

    Regards,

    Sunny.

  • The building has successfully completed and there is nothing left to care about.