Part Number: DRV602
Hi Sir,
I want to use DRV602 to replace MAX97220AETE, Would you please help review below circuit change to DRV602?
VDD=5V, is there have any relative resistor and capacitor need change?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV602
Hi Sir,
I want to use DRV602 to replace MAX97220AETE, Would you please help review below circuit change to DRV602?
VDD=5V, is there have any relative resistor and capacitor need change?

Hello,
I will review this schematic with my team and have feedback for you shortly.
Best Regards,
Justin Beigel
Hi Jeff,
These two devices are not exact replacements. External components and connections can be used with DRV602, but package and pins are not the same.
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators