Part Number: DIR9001
Hello,
I am trying to use the DIR9001 in PLL-only-mode, according to the schematics below.
When I apply an optical signal to my TOSLINK receiver, the PLL locks, and I get valid outputs on FSOUT0/FSOUT1, depending on the input format. I tried with 44.1 kHz and 48 kHz inputs, and in both cases the LRCLK and the BCLK are generated correctly. However, I never get any DOUT signal (always low -> MUTE). The ERROR pin is high, so there is probably some parity/data error, since the PLL locks fine.
What could be wrong? The optical sources work fine with other equipment.
Thanks in advance