Hello,
I have a question about pop noise after Class-D speakers on.
If the Class-D speaker is turned on after the wait is set for 3 ms after the WCLK operation is started, pop noise will occur.
However, when the weight is set to 3.75ms, pop noise does not occur.
At this time, the sound sampling frequency used is 8kHz (125us).
What should be the wait time between turning on the WCLK and the Class-D speaker?
Best regards,
Nomu