Part Number: TAS5825MEVM-SB
Other Parts Discussed in Thread: TAS5825M, PP-SALB2-EVM
Hello,
I am starting to evaluate your TAS5825M product and am quite interested in using the speaker characterization for improved performance. I had no problems importing the frequency response SPL data for the woofer and tweeter but it seems there is no way to import measured data for the impedance curves etc. I have read about the "learning" EVM but it seems it is geared towards much smaller drivers as those used in tablets, laptops etc.
My application is a two way (woofer & Tweeter) system comprised of a 5 inch woofer and a 3/4 dome tweeter and I was hoping to use some of the advanced functionality that the TAS5825M offers in its DSP processor. My question is this; Is there a way to import characterization data directly into the Purepath console from other tools other than the PP-SALB2-EVM learning board?
If the PP-SALB2-EVM is absolutely required, will the characterization data be useful in my application? At a $999.00 cost I need to know if it will provide useful data.
I look forward to hearing your comments.
Best regards,
Jim Albert