There are 3 Biquads in TLV320ADC3140. Can we use them just to add some delay to the audio signal chain so as to adjust the whole signal processing latency?
If we disable one of these Biquads then the latency of this Biqauds will be Zero? If we enable one of them, the maximum delay we can get is 2 samples?
The datasheet specifies the latency of internal Digital Decimation Filters clearly, but what is the overall latency if we turn off all the Biquads and set the Channel Phase Calibration to Zero?