Other Parts Discussed in Thread: DRV632, TLV320AIC3104, TPA3113D2
Hi
I would like to have a solution of Audio codec differential line out convert to single-end out.
Do you have any suggestion IC for this circuit ?
Thanks!
Sincerely,
Chin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Chin,
Our team is looking into this and will respond as soon as possible.
Best Regards,
Justin Beigel
Hi Chin,
Can you provide further description of your required system? You want to take a differential signal input into a single-ended output? Devices like DRV632 may be useful for this.
However you mention Audio codec, do you need digital audio interface?
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Hi Ivan,
Thanks for your answer. Attached is our block diagram of Audio system. Refer to the block diagram, could you please provide the suitable TI solutions to us ? Thanks!
1. Audio codec --- Need Linux kernel 4.4 supported.
2. Amplifier ---Class-D 5W@ 8ohm. Amplifier output must be short-circuit protected.
3. Single-end to differential converter.
4. Differential to single-end converter.
5. Driving buffer (see the yellow color int he block diagram).
6. In the block diagram, there are two voice source inputs (see the blue color) connect to Line_in_L+/-. Does TI have solution to do such
design ? I worry about if directly connect both sources (voice source 1 and voice source 3) to Line_in_L+- and without any circuit, maybe
we will meet audio issue in this kind of connection.
Thank you for your help!
Sincerely,
Chin
Hi Chin,
Let me comment below:
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Hi Ivan,
Thanks for your answer.
About Audio codec , I checked the TI portfolio and I think TLV320AIC3104 can meet our block diagram requirement.(We also need AGC function) . I would like to know , does TLV320AIC3104 can be supported in Linux kernel 5.10.9 ? software driver ready ? Our platform is embedded Linux system.
Thanks!
Chin
Hi Chin,
Let me check on the supported versions for this device. Will provide some updates tomorrow or Monday night.
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Hi Chin,
Please refer to this site for driver details: TLV320AIC3XSW-LINUX Driver or library | TI.com
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Hi Ivan,
Okay, Thank for your information!
By the way, We decide to design TPA3113D2 to drive our Mono speaker (5W/8ohm).
Following questions need your help to answer.
1. If our audio source is Mono input, can we connect just only one channel (Left_in and Left _out) to fit our requirement ? or We have to connect
as PBTL architecture (Figure 39 of datasheet) ?
2. Which efficiency table can be referenced if we design Mono speaker ?
Thanks!
Sincerely,
Chin
Hi Chin,
Please start a new thread for TPA3113D2 as it belongs to a different team, this way the responsible team will be able to check your questions.
Some comments in advance I can provide:
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators