Part Number: PCM1802
The lack of PSR data for this device is a hindrance. The datasheet just says that VCC should be clean. What does that mean? A battery?
I have a clean VREF2 (-106dBu) but my VREF1 (midrail) is much noisier (-85dBu) for some reason, causing out of spec ADC performance . The datasheet suggests VREF1 is derived from VREF2 and I do have all of the recommended decoupling so I am not sure I understand the reason.
My VCC rail is noisier @ -55dBu so I am assuming this is affecting my VREF1? Not sure why it should though if my VREF2 is supplied is clean,
Has anyone managed to achieve the SNR performance of 105dB? No eval board avalaible.