Hello,
Our customer is facing lower channel separation performance at HP-output.
Using EVM, observed clear performance difference caused by common mode voltage setting at 3.3V HP power as below.
P1,R10,D4-6 1KHz FSR L to Rch R to Lch
Common mode=Full chip 108.0dB 108.2dB
Common mode=1.65V 74.4dB 82.4dB
Common mode=1.65V(Remove AVDD bypass cap) 80.2dB 89.2dB
It is interesting that AVDD cap made 6dB difference, it seems power line is so sensitive.
How can we get 100dB over separation using LDOIN(HPpower)=3.3V and Common mode=1.65V configuration?
Regards,
Mochizuki