Part Number: SRC4192
Hi Team,
In slave mode, SRC4192 output port BCKO need to input a clock from external device, it may operate at rates from 32fS to 128fS, does BCKO set to 64fS also okay here? We try to offer BCKO = 3.072MHz, and LRCKO = 48kHz, given SDIN message by APx500 but we can't get the correct output at SDOUT. Any problem of my usage? Confirm the AP receive side already set to 32 bits Per channel. Could your share 1 application example of SRC4192 slave mode? That would help us to bench test easier. Thanks.
Related pin setting:
IFMT 2 / 1 / 0 set to 0 / 0 / 1, means input is 24 bit I2S.
OFMT 1 / 0 set to 0 /1, and OWL 1 / 0 set to 0 / 0, means output is 24 bit I2S.
MODE 2 / 1 / 0 set to 0 / 0 / 0, means both input and output are slave mode.