Part Number: PCM3168A
Other Parts Discussed in Thread: TIDA-00609
Hi,
I am using PCM3168APAP in my design. I referred to the Figure 58,59,60and 61 and observed while connecting input signal to buffer it is connected via electrolytic capacitors. I referred to DEM-DAI3168A schematics. It has electrolytic capacitors connected.( Eg Designators:C601,C607,C501,C502). When I referred the TIDA-00609 it has ceramic capacitors connected at input of buffer.(Eg Designators: C200,C207,C241,C242). Which one is the correct selection of capacitor. Whether we should consider electrolytic or ceramic capacitors. My audio sampling frequency requirement is 48kHz
2. There are different system connection mentioned in section 10.3. Is there any reference example for Differential to Differential Buffer