Other Parts Discussed in Thread: LM386, TPA3138D2
Hi Team,
NE5532 audio amplifier, the application of loudspeaker 8Ω single-ended amplification. Output wave distort when carrie the Load,while not carrie the load, the wave is ok.
thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

1. schematic

2. No load, test between C6 pin1,2.

3. Carrie the load.
Hello,
The NE5532 is a audio signal amplifier capable of 600 ohm load. It does not perform well with 8 ohms or 33 + 8 ohms. NE5532 has a current limited output.
Other note, 33+8 ohms and 10uF only goes down to 400Hz.
Would you like a speaker driver IC recommendation?
Hello,
Is there any solution to solve the application with 33+8 ohms loads? could you help to explain the distort wave in the C6?
thank you!
There would be less voltage loss across the capacitor if it was a larger capacitance value. Notice that yellow follows the blue on the blue edges (high frequency >> 400Hz) and the yellow falls on the blue plateaus (low frequency <400Hz)
To drive the load there is the simple and classic (old) LM386 and the much newer (modern) TPA3138D2
Hello Guo,
You can double the output current capability by using both channels. Minimum output "short" current is 10mA (that is 25C, hotter will lower this current). Assuming a 4V loss on NE5532 output leaves 8V or +/-4V. 4V/20mA = 200 ohms.
Therefore, add a impedance matching transformer (high impedance) to 8 ohms. Or pick a higher impedance speaker.
https://www.digikey.com/en/products/detail/pui-audio-inc/AS015100MR-R/11618406
Add the two outputs like this. The speaker above (still an op amp overload at high output) will work much better than an 8 ohms speaker (major overload). Lastly don't put this into production, but OK for personal use.

If you have to use 8 ohm speakers, How many can you put in series?
With just one 8 ohm speaker, use both amplifiers and combine them per the previous picture. Then see how loud it can go before distortion (clipping) becomes an issue.