Hi team,
It's mentioned in a book that“One of the most useful techniques in low-noise electronics is to use two identical amplifiers so that the gains add arithmetically, but the noise from the two separate amplifiers, being uncorrelated, partially cancels. Thus, we get a 3 dB noise advantage each time the number of amplifiers used is doubled. ”
In order to prove this conclusion, the book uses 5532 to increase the number of differential amplifiers in pairs and the number of input buffers for noise test. The circuit diagram is shown in (a) (b) (c) (d). The results are shown in the table below. The noise will indeed decrease with the increase of 5532.
Could you please help analysis the reason about why noise will indeed decrease with the increase of 5532? Is there any other disadvantage in increasing the number of 5532 in pairs?
Best Regards
Wesley Huang