Part Number: PCM3168A
Hi,
I am using PCM3168APAP Audio Codec in my design. I have attached the schematics. Can someone please review the schematics and let us know your feedbacks on the same8510.Audio Codec.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM3168A
Hi,
I am using PCM3168APAP Audio Codec in my design. I have attached the schematics. Can someone please review the schematics and let us know your feedbacks on the same8510.Audio Codec.pdf
I will take a look at it and let you know. by the endo f tomorrow.
Regards,
Arash
Hello, I looked through your schematic and I only noticed you are using RST_N and tied it to active High , where as in datasheet it is RST which is Reset and power-down control input with active low.
Kind Regards,
Arash
Hello, based on datasheet it needs to be active low not active high.

you can also take a look at EVM documentation for this part to better understand the usage and general connections at:
Regards,
Arash
Hi,
Can you please let me now at what impedance VIN+/- and Vout+/- should be routed if its configured as differential. Should 100ohm impedance be ok.
At what impedance VIN+/- and Vout+/- are routed in DEM-DAI3168A EVM
Hi Shifali,
100ohm should be OK. As long as layout on both sides of the differential connection are as balanced as possible, the actual load would be the circuit the input or output is connected to, eg. a filter, an amplfiier, etc.
Best regards,
-Ivan Salazar
Applications Engineer