Hello Guys,
Good day.
Need your help guys on the requirement from the customer below:
"I need your IC for controlling two speaker through one input spkP and spkN. Both speaker have 8ohm and 2watt rating. The input to them is from Qualcomm based SOC, which can support upto 1.9watt power.
I have single input with 1.5watt so i want to run two speaker with them of ratting 2watt.
if I have to use two speaker and connect them in parallel it would half the impedance from 8ohm to 4ohm. And would double the power. I want to get same 2watt and 8ohm on both speakers."
Thanks and regards,
Art