Hi all,
Im facing a issue with the SRC4392, it seems that once i connect the board that houses SRC4392 my I2C bus is broken. SDA/SCL is repectively pulled high by 3k3 resistors each one the board containing ESP32. There is an ADAU1467 on the same I2C bus which i can communicate with as long as the board with SRC4392 is disconnected. Doing a quick measurement i can see that the SDA is pulled down (20mV) which ofcourse will destroy the bus. Disconnecting the board and communications are fine again. Im attached my schematic, anyone who could see if ive made a mistake here? Ive been reading the datasheet but i cannot find anything wrong.. RST is pulled high so the device should be active.
Thanks,
Stian
digiboard_schem.pdf