This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DIX9211: Operation when AC3 data or DTS data of DIX9211 is input

Part Number: DIX9211


I am considering an alternative to DIR IC, and please tell me about the behavior when AC3 data or DTS is input to DIX9211.
In the IC before the change, regardless of whether the input data is linear PCM or compressed audio, the data corresponding to the Audio Sample in the subframe of SPDIF is output in I2S format and processed by the DSP in the subsequent stage.
Is it possible for DIX9211 to output the data equivalent to the Audio Sample in the SPDIF subframe on the 1ch I2S format to the subsequent stage for data such as AC3 data and DTS?