Part Number: PCM3060
Hi,
The customer connects an inverting amplifier to the DAC output.
They want to know the load drive capability as they connect a resistor to the input of the OPAMP.
/OPAMP configuration is below.
Inverter amplifier, amplitude = 4V (0.5-4.5V), Gain = 2, Single end input
What is the load that the DAC output can be used without distortion?
In the simulation, the same 10k as the EVM is connected, so it is about 0.4mA.
Is this safe enough? When 4.7k is connected, it becomes 0.85mA. Is this a problem?
Best regards,
Hiroshi