Part Number: TAS5754M
Hi Team,
How to use I2C control part in fast and low mode?
BR,
Gust
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gust
There's no register to specially control the I2C in which mode. When you use I2C in Standard or Fast mode, please take care of the signal requirement in the datasheet, as the table below. For example, if you use SCL clock higher than 100kHz, the I2C should work in Fast mode. In this case, the Rise time, the Fall time and other parameters must accord with table 7.10. Thank you.