Part Number: PCM1803A
Hello,
It is not clear which of REF1/2 is for L/R channel. Is REF1 for L channel as the diagram in top page of datasheet implies?
Thanks!
Regards,
Oguri
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM1803A
Hello,
It is not clear which of REF1/2 is for L/R channel. Is REF1 for L channel as the diagram in top page of datasheet implies?
Thanks!
Regards,
Oguri
From the Datasheet I could see the following. While i am not 100% sure I make the below inferences.
1.Vref1=0.5*Vcc or a center voltage of 2.5v
2. Vref2 to GND voltage was a voltage equal to the analog full scale voltage. As per datasheet 0.6*Vcc=3vpp is full scale range. The Vref2 should then be a DC voltage of 3v