Part Number: TS3A227E
Hi,
Would you please help help review below TS3A227E design?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeff,
I will message you my email shortly after the reply - as the full schematic + layout will be necessary to do a full review on the board.
Please ensure that the audio jack connections are also shown in the schematic so I can verify those connections on the jack side as well as the IC.
I don't see any major concern so far - but I do have a couple notes:
1. R413 is unnecessary and I'd recommend a direct connection to the CODEC ground (which could be the same as system ground depending on system)
2. We recommend 2 supply decoupling capacitors - one 1uF and one 0.1uF, so I'd suggest adding a 0.1uF cap to the power supply in addition to the 1uF already there.
We can continue the discussion offline - I will follow up with my email in an E2E message.
Best,
Parker Dodson