Part Number: PCM9211
Hi
I am working on a design that uses the PCM9211 for S/PDIF input and output.
I am providing a 24.576 MHz clock into the XI pin and a suitable S/PDIF signal into input pin RXIN3, and I reset the chip(s) with a low pulse on their nRST pin.
I have an IIC connection and can read/write the registers and the reset values are as described in your datasheet.
I have changed register 0x34 to 0xC3 to select my input pin (RXIN3), all other registers keep their power-on RESET value.
I am monitoring the output pins SCK0, BCK, LRCK and DOUT expecting to see a decoded I2S version of my input.
The clocks are outputing perfectly correctly, and change frequency if I change the sampling rate of my S/PDIF transmitter from 44.1kHz up to 192 kHz
_BUT_ there is no data coming out of the DOUT pin.
I have tried changing register 0x6B to 0x11 to avoid any possibility of Automatiic selection confusing me with switching to the ADC (which I am not using).
Further confusion comes from registers 0x38 and 0x39 which both read as 0x00 - suggesting the incoming S/PDIF is "out of range" but if this is so why are the clock output pins tracking my S/PDIF generator ?
I hope you can suggest something that I can check to find out why I have no output data.
Thanks for your time
Kind Regards
PhilipJ