This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5720MEVM: The TAS5720M EVM is no longer recognised when it is connected to computer and fault LED is on when PVDD is connected

Part Number: TAS5720MEVM


Hello,

A couple of days ago I have followed the procedure in the Chapter 2 in the user's guide and the device worked as expected when it was connected to a computer using the USB cable.

When I was trying to use the I2C/I2S communication on this device with Linux without a USB cable plugged in I encountered an issue, the fault LED was turning on whenever I was turning on the power supply for PVDD. This wasn't happening earlier when it was connected with the USB.

I was trying to resolve this issue, and later on when I tried to connect the device again to a computer with the USB cable, the device was not detected/recognised by my computer. I can see that the device is powered up since the 3.3V green LED and the USB LOCK blue LED light up. I tried to connect it at a different port and with a different cable but the problem remained.

Also, now whenever I turn the power supply for the PVDD on, the fault LED turns on, which was not the case earlier with a USB connection (it only happened while trying to use use the I2C/I2S communication). The power supply used for PVDD it was set either to 5V or 10V.

I hope that someone can help me on why the device is not detected by my computer anymore, and why the fault LED turns on whenever PVDD is connected to it

Thanks in advance,

Theo