This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5805M: TAS5805M test problem

Part Number: TAS5805M


Hi Ti Team,

We found that there is a phase difference between the left and right channel outputs of the TAS5805M, which is 5° when the programming bypass software plays 1kHz audio, and 45° when playing 10kHz. At present, there are three machines that have this phenomenon, and the error of the component device can be eliminated. Is this normal?