Hello, TI
I have a few questions.
I'm trying to use a differential mic, line in and out. Please check the diff mic input and other circuits are good.

When using the above circuit, how to set the register?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, TI
I have a few questions.
I'm trying to use a differential mic, line in and out. Please check the diff mic input and other circuits are good.

When using the above circuit, how to set the register?
Thank you.
MIC CONNECTIONS ARE FINE.
I enclose blow a script that can enable the Mic and speaker circuits.
https://www.ti.com/lit/zip/slac366 This is link to a GUI for the EVM.
# --------------------------------------------------------------- page 0 is selected
w 30 00 00
# s/w reset
> 01
# PLL_clkin = BCLK,codec_clkin = PLL_CLK
w 30 04 07
> 91
> 20
> 00
> 00
# mode is i2s,wordlength is 16
w 30 1b 00
# NDAC is powered up and set to 4
w 30 0b 84
# MDAC is powered up and set to 4
> 84
w 30 12 84
> 84
# DOSR = 128, DOSR(9:8) = 0
> 00
# DOSR(7:0) = 128
> 80
# DAC => volume control thru pin disable
w 30 74 00
# DAC => drc disable, th and hy
w 30 44 00
# DAC => 0 db gain left
w 30 41 00
# --------------------------------------------------------------- page 1 is selected
w 30 00 01
# De-pop, Power on = 800 ms, Step time = 4 ms
w 30 21 4e
# HPL
w 30 1f c2
# LDAC routed to HPL
w 30 23 40
# HPL unmute and gain 1db
w 30 28 0e
# No attenuation on HP
w 30 24 00
w 30 25 00
# MIC BIAS = AVDD
w 30 2e 0b
# MICPGA P = MIC 10k
w 30 30 40
# MICPGA M - CM 10k
> 40
# --------------------------------------------------------------- page 0 is selected
w 30 00 00
# select DAC DSP mode 11 & enable adaptive filter
w 30 3c 0b
w 30 00 08
w 30 01 04
w 30 00 00
# POWERUP DAC (soft step disable)
w 30 3f d6
# UNMUTE DAC
> 00
# POWERUP ADC channel
w 30 51 80
# UNMUTE ADC channel
> 00
w 30 00 01
# Unmute Class-D Left
w 30 2a 1c
# Power-up Class-D drivers
w 30 20 c6