Dear ,
I check the basic mode & smart amp mode on SLAA653A , Is the basic mode one of the smart amp modes?
the basic mode will protect the woofer or full-range speaker ,so i can write the calculated on the page 0 ,Register 61 & 62 .
3.1
Basic Mode allows playback to the laptop loudspeaker without exceeding its power handling
specification. It simply configures the TAS5766M with no processing and a fixed output level.
As explained in the PurePath Smart Amp Design Guide, the peak amplitude corresponding to
a particular loudspeaker power handling level can be calculated by the following equation:
Regards,
bard