This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3204: Headset detection

Part Number: TLV320AIC3204


Hi Sir,

We are currently experiencing a problem with the headset detection function of TLV320AIC3204. When a 4-segment earphone is inserted, after a slight pause (about 0.5s), the earphone will be recognized as a 3-segment earphone, which makes it impossible to using the MIC to record voices. I have tried to set the anti-shake time recognized by the headset to the maximum 512ms, but it does not work. 

Do u have any good suggestion for this question?

Thanks,

Best Regards