Hi,
I'm trying to use the tpa3255 to check the largest output power without triggering OTP.
BTL connection with condition below:
Pvdd:48V, Gvdd:12V; Rload=2ohm;
I noticed that the OT is triggered when output power is about 100w( output current 7A * rload voltage 15v). does this result meet the design spec ?
And also could you please share some useful heat dissipating method?
hi sam, in idle status, duty cycle is around 50% and no overlap is found. under PBTL config, how is the feedback loop working?is it separately or independently?