Part Number: PCM4202
Other Parts Discussed in Thread: PCM1804
Hello team,
I received a question from the customer about audio data format of PCM4202.
① Relation between audio data width and BCK clock
When the PCM4202 is set to PCM Slave mode, does the width of the 1-bit audio data output depend on the clock of the BCK that is supplied externally to the PCM4202?
For example: If BCK is 64FS when FS=48kHz, the BCK's 1-bit width is set to 1/64FS[s]; if BCK is 128FS, the 1-bit width is set to 1/128FS[s].
② Confirm of what frequency should be entered to BCK
When the PCM4202 was set to PCM Slave mode and Single Rate Sampling mode, the data sheet was written to enter 128FS in the BCK. Would you confirm if this is correct? (Datasheet p16)
With other ADCs, they have seen BCK set to 64FS well, and they have never seen an ADC set to 128FS, so I want to check it just in case.
③ Data format difference between function compatible devices
The PCM4202 is a function compatible product of the PCM1804 pin-control, but there is a difference in the data format when the audio data is at the PCM output.
When set to 24bit Left Justified, the PCM4202 is left justified from the MSB, while the PCM1804 is left justified from the LSB.
Is it convenient to recognize that there are differences in data formats even in functional-compatible products?
Please contact us if there are more information needed.
Best Regards,
Ryotaro Fukui