Part Number: TLV320AIC3104
Now I use TLV320AIC3104 in imx8mm,because imx8mm's DMA isn't opend,when i use aplay commond ,the log is down

root@imx8qxpmek:~# aplay --device default:CARD=imx8mmevkcodec Front_Right.wav
Playing WAVE 'Front_Right.wav' : [ 7169.215073] tlv320aic3x-codec 1-001b: Unable to sync registers 0x3-0x3. -6
Signed 16 bit Little Endian, Rate 48000 Hz, Mono
[ 7169.278333] imx-sdma 302c0000.dma-controller: sdma firmware not ready!
aplay: pcm_write:2061: write error: Cannot allocate memory
So I want to ask must the TLV320AIC3104 need the DMA control?