Part Number: TAS5624A
Other Parts Discussed in Thread: TAS5624, , TAS5825P
Hi,
I am using dynamically control PVDD supply to TAS5624 ( class G supply method). This dynamic PVDD is controlled by output of AMP CLIP signal of TAS5624 to control the feedback of boost converter that supply TAS5624 PVDD. My lower PVDD is around 17V and higher PVDD is 36V.
When the output signal reach near clipping, the AMP CLIP will start to turn "LOW", then my PVDD move to higher voltage. My amp configuration is 2.1. 2CH for front speaker which is single ended(SE) configuration and woofer as BTL.
During the supply from low supply switch to higher supply, the SE channel output will clip for about 23ms. After some study, I found out that the output clip during supply switching is due to TAS5624A output bias level( PVDD /2 ) react slowly compare to the PVDD. PVDD takes 2-3ms to raise from Low to High, but the AMP output takes 20 ~ 30ms to raise the bias to PVDD/2 which cause clipping at low side of signal.

May I know the why the Bias of AMP output raising slowly as compared to the PVDD raising speed?
Besides, do you have recommend High power class d amp (150W above per BTL) that support dynamic PVDD ( whether is Class H or Class G supply) without happen any clipping during supply switching?
Thank you