This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1864: Max sampling frequency

Part Number: PCM1864

Are sampling frequencies greater than 192kHz achievable for this device?

Desired sampling frequency: 196608Hz

  • Hello Connor,

    It could be possible given you are using external clock source and not PLL and set LRCK and BCK ratio appropriately as well as disable the clock error detection, but it would be operating out of spec and cannot attest to the performance the datasheet guarantees if you choose to do that to get a higher sampling rate.

    Best Regards,

    Carson 

    Low Power Audio Applications