Part Number: PCM5122
Other Parts Discussed in Thread: PCM5142, SRC4392,
DAC team,
Our customer is trying to get a THD+N reading similar to the datasheet. They get -91.5 dB on the left channel which they can accept, but the right channel is at about -90 dB. Maybe it's a matter of setup, so I asked for details about the test setup, which I'll list below.
Please let me know what you recommend.
There are just 3 cables:
- Audio Precision APx525 Optical out -> PCM5122EVM Opto SPDIF in
- PCM5122EVM OUTR (or OUTL) -> APx525 Analog Input 1 (Unbalanced) using RCA cable (~1m) and an RCA-BNC adapter
- USB connection to my laptop docking station for power and control
The laptop is in a docking station and AC powered.
See images in the .7z file attached.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/6/EVM-Setup-Pics.7z
Configuration notes:
- Jumper W5 on pins 2&3 to select RXCKO
- Configure SW3 as HHLX (A-D) – MCLK #4, 24.576MHz from Osc Y2
- Use PurePath Console v1.16 and select PCM5142 EVM
- Use Direct I2C Access to load and execute “Optical/SPDIF Input via J4 (48 kHz, RXCKO Master Clock)” script from EVM user guide (section 2.5.3)
- Script file I use attached here as PCM5121EVM_SRC4392.txt (copy/paste from EVM user guide)
Everything else is default.
Observations (quoting the customer):
- To get better than -91dB THD+N on the “good” EVM channel OUTL, I had to disable the PLL in the PCM5122, and mute the Audio Precision digital output channel associated with the EVM OUTR
- Seems like there is a bit of crosstalk on the EVM somehow? Improvement in THD+N by muting the input associated with OUTR was ~1dB at 1kHz
- OUTR THD+N performance was NOT noticeably improved by turning off the OUTL input
- OUTR as is doesn’t meet the -90dB THD+N target
He saw a small improvement (~0.2dB) in the THD+N performance on both channels when he disabled the PLL in the PCM5122 (cleared bit 0, register 4, page 0).
OUTR THD+N measurement (1kHz, -1dBFS, High Pass filter = AC (10Hz), Low Pass filter = AES17)

OUTL THD+N measurement (1kHz, -1dBFS, High Pass filter = AC (10Hz), Low Pass filter = AES17)

Clocks are:
TP13 LRCK = 48.00kHz
TP11 BCK = ~3.072MHz
TP10 SCK = ~24.576MHz
Register settings:
# RESET RESET THIS IS MASTER RESET FOR SRC # SW3 (2-7) turned on, rest turned off # Page 0 = DEFAULT for Control # Write to page 0 w E0 7F 00 # Register 01, Bit 7 = 1 resets to default d 100 w E0 01 80 # Delay 0.1 sec to allow part to reset d 100 # Register 01, Bit 7 = 0 for normal operation w E0 01 00 d 100 # w E0 7F 00 # Register 01, Bit 7 = 1 resets to default #----- Setup Port A ------# # 24bit I2S, Master mode, DIR source, at mute # Divide by 256, MCLK input source w E0 03 69 w E0 04 0B #----- Setup DIR ------# #DIR Config 1 # Input source: RX2 - S/PDIF RCA (default) #w E0 0D 01 # Input source: RX4 - S/PDIF optical, RX_MUX = RX1 w E0 0D 08 #DIR Config 2 - default w E0 0E 01 #----- Setup DIT -----# # DIT COnfig 1 # Port A data in, DIv 256 w E0 07 80 # DIT Config 2 # Default is to output to RCA # Commment out RCA and uncomment Optical for optical outputs #Output to RCA # TX - ON, TX MUTE - ON, Optical disabled #w E0 08 06 # TX Mute - OFF #w E0 08 04 #Output to Optical # TX - OFF, TX MUTE - ON, optical disabled w E0 08 03 # TX MUTE - OFF w E0 08 01 #----- PLL Configuration -----# # Set P=2, J=8, D=0 w E0 0F 22 w E0 10 1B w E0 11 A3 # GPIO1 Config # GPIO1 = RCVR non-audio data w E0 1B 06 # GPIO2 Config # GPIO2 = RCVR non-valid data w E0 1C 07 # Power Status # Disable RCVR (/PDRX) and Port B(/PDPB) power down and enable All Function power down #w E0 01 14 # Unmute Port A Output w E0 03 29 # Disable All Function power down (all blocks set by local control) w E0 01 3F
Thanks,
Darren