This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5805M: Thermal Question

Part Number: TAS5805M


Hi team,

I would like your help to answer below question.

1. Jucntion temp calculation

Users wants to calulate junction temp for local standards. If customer measure the case top temprature, Tj will be calculated as  Tj = Tc + (ψJT * Power), correct?

They are measureing the temprature at TC1 of the picture

In addition, how to calcurate Power in such a class D amp IC?

2. The way to reduce Tj

Users wants to have lower temprature in the system.

With PVDD = 12.6V, Fs = 384kHz, currently TC1 is 105℃

Could you suggest any way to reduce power consumption?

Regards,

Hideki