Part Number: TLV320AIC3106
Hello,
I'm designing a device using the TLV320AIC3106. I'd like to have the option for microphones that require Phantom Power to be connected to the device.
On the development module, the inputs have a single .1uF capacitor on the positive and negative inputs of the lines/mics.

I read the TI design note called Phantom Power with Operational Amplifiers. From that note, I designed the following schematic.

Will the change from a 0.1uF bi-polar cap to a 10uF polar cap work correctly to connect a dynamic or condenser microphone to the '3106? Does my schematic make sense?
Thanks for the sanity check!
Jay