Part Number: PCM1865
I am using the PCM1865 in a 24 channel recorder for air traffic control. For this I will be using 6 PCM1865 devices. I would like to connect them in 3 pairs, 3 masters and 3 slaves. I intend to distribute a single crystal output to the master SCK1 inputs and then use the BCK and LRCK outputs to drive the slave devices. All devices will be driven at 48KHz sample rate with a 24 bit resolution. The outputs of each pair is TDM 10 channels (4 A/D outputs with their associated secondary A/D channels).
Is their a method to connect these 6 device to use a common LRCK? As the TDM inputs are to fed into an FPGA for processing it would save a lot of hassle if they shared a common LRCK.
Thanks