Part Number: PCM1864
Other Parts Discussed in Thread: TMUX1308, PCM1860, TMUX1309
Hi Team,
You've helped us to put on our customer to decide on PCM1864 as it takes 4 analog stereo audio and outputs 2 independent digital I2S audio. They saw that it uses the same WS and CLK signals for both channels despite being fully independent from each other. However, they've come across a few follow-up questions:
Can I use other I2S audio devices with their DOUT signal while using my WS and CLK from PCM1864? Or should they have their own independent CLK and WS lines... assuming all 192khz?
My real world case is an HDMI transmitter IC which can have multiple I2S audio inputs but has only one CLK and one WS inputs... and I have different sources of audio in my board... analog audio to converter by PCM1864, and also separate digital I2S audio coming from HDMI receiver ICs and external connectors.
Can I take CLK and WS from PCM1864, and just take the DOUT from all these sources? Or should they be with their own independent CLK and WS?
If they should have their separate independent CLK and WS, then I thought of using 3 TMUX1308 to choose select the desired input... one TMUX1308 to pick the required I2S DOUT signal, one for WS, and one for CLK.
Please advise for this issue + if separate signals are required, will the TMUX1308 be a good apprach? Is TMUX1308 suitable for audio signals here?
Thanks in advance!
Kind Regards,
Jejomar