Part Number: PCM1808
Hello Expert,
I have questions for PCM1808.
This device's SCLK accept following frequency under master mode.
| min | typ | MAX | Unit | |
| 256fs | 2.048 | 12.288 | 24.576 | MHz |
| 384fs | 3.072 | 18.432 | 36.864 | MHz |
| 512fs | 4.096 | 24.576 | 49.152 | MHz |
My understanding for this table, this just showed what fs can be used.
For example, 96kHz is highest sampling frequency under 512fs case.
This because, if it is actual min/Max, there isn't margin for upper and lower limit fs from the point of view of frequency variation.
Therefore, I'd like to know about frequency variation tolerance for SCLK.
Then would you tell me margin for expected SCLK frequency?
Also, I think device will be into Clock-halt power down when SCLK frequency variation exceed above tolerance.
Is this understanding correct?
Best regards,
Kazuki Kuramochi