Hi Guys,
Could you tell me, what is the difference between TAS5630 and TAS5630B version? Anything better/worst?
Best regards,
Tomasz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tomasz, the differences are these.
- DC offset improved by a factor of about 3 (50mV max vs. 150mV max, to improve turn-on/off pop in some cases).
- OUT_C-D crosstalk improved to match OUT_A-B.
- Internal oscillator disabled in SLAVE mode (eliminate potential for low-level tones in the noise floor).
- CLIP indication disabled during RESET and turn-on ramp (eliminate potentially confusing indication).
Regards,
Steve.
Thanks Steve,
So unfortunately the output noise performance isn't improved ... TAS5630 would be a great chip having the output noise on the 100µV level...
Tomasz
Steve, when will the TAS5630B be available in the DKD package? Will it be a separate part number from the TAS5630?
Russ
Russell, TAS5630B is scheduled for releast to market in August. Samples should be available about a month before that. It will be called TAS5630B (that is, either TAS5630BPHD or TAS5630BDKD).
Regards,
Steve.