Part Number: PCM1808
Dear Expert,
I have questions for SLCK of PCM1808 when a “Master mode”.
I understand there are limited by 512fs just for about less than 4MHz or higher than 53.33MHz.
Except for that situation, PCM1808 activates well because frequency was just decided.
Is this idea correct?
My customer wants to spread SCLK like 24.576MHz ±3MHz.
If it was correct, when PCM1808 is used as a “Master mode” for 512fs, System Clock Frequency (SCLK) can be acceptable for 4.096 to 49.152 MHz.
In that case, SCLK should be about 21MHz < SCLK < 28MHz and this is within the above range.
Therefore, is it possible to active correctly without hanging etc.?
Thank you.
Koki Tsushima