We have a product using PCM3168A which has been in production for over a year. Recently we've been getting a number of failures (in the field, after sale).
The symptoms are that the generated audio clocks are at the wrong frequency, and only 1V in amplitude.
We run the codec with the ADC as master, set to 256x fs, and the DAC as slave. The system clock is 24.576MHz, so we expect a 96kHz LRCLK.
When the part fails, we get a 64kHz LRCLK, and as I say the output LRCLK and BCLK signals are only 1V.
Is this a known issue?