This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2700EVM-HV500: Regarding the trigger button

Part Number: DRV2700EVM-HV500
Other Parts Discussed in Thread: LDC3114, DRV2700EVM

Hi, 

DRV2700EVM-HV500(EVM) has a trigger button for operation without using GUI. In order to use a trigger button, the MSP needs to be programmed. Could you write a program so that EVM can apply voltage to piezo triggered by electromotive force which comes out of pressed piezo?  If it can not, it seems that you need LDC3114 to detect the pressure and trigger EVM. But I have no idea how I should connect those two devices.  

Best Regards,